{}
搜尋常見問題
Video: How can you set up the ATV61 or ATV71 drives Multi motor configuration with the SoMove software?
Issue:
ATV61 or ATV71 Multi motor configuration with the SoMove software

Product Line:
Altivar ATV61 and ATV71 using SoMove Software

Environment:
All

Cause:
Where do you find the ATV61 and ATV71 multi motor settings using somove software

Resolution:
Open up SoMove and install an existing or create a new project if needed choosing the ATV61 or ATV71 drives.
Once you have the project open choose Device at the top of the screen. Scroll down to choose multi configuration switching.  This will open up a window that allows you to assign the logic inputs for Multi motor or Multi configuration.
Choose Multi motor by checking the circle
Now you can assign your logic inputs example LI4 and LI5 as inputs to switch between Config 1 and Config 2.
Now Config 1 and Config 2 are no longer grayed out and can be configured for your multi motors by choosing motor control and setting up your motor parameters for each configuration.

The following video demonstrates this process:

.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: