{}
搜尋常見問題
Generic_Modbus_DDXML_DTM_Library_2.0.3 documentation
Title
Generic Modbus DDXML DTM Library 2.0.3 documentation

Issue
Generic Modbus DDXML DTM Library 2.0.3 documentation

Product Line
Modbus

Environment
Unity

Cause
N/A

Resolution
The ReadMe file for Generic_Modbus_DDXML_DTM_Library_2.0.3 states that for devices supporting only Modbus serial line communication Process Data tab will not be available.
The Process Data tab is unavailable for device DTM which supports Modbus serial line protocol because some device DTM does not have Input/Output process data, as the DDXML does not contain the information for the process data. Attached is the documentation.

施耐德電機Taiwan

附件
User Manual Generic_Modbus_DDXML_DTM.zip [3.44 MB]
探索更多
系列:
可能有幫助的文章
探索更多
系列: