我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
        
我們今天可以如何提供協助?
Cannot find the UA OPC Tools in OFS
Issue
The option to install the UA OPC tools cannot be found during the install of OFS 3.6, SP1.

Product Line
OFS

Environment
Windows 10


Resolution 
The option to install the UA OPC tools cannot be found during the install of OFS 3.6, SP1.

The UA OPC Tools (UA Client, UA Configuration, UA Wrapper) were never meant to be used by the customer. The 
tools were intended for development only and have been removed from OFS as of version 3.6, SP1.