{}

我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
Is it possible to send the status of VIP410 watchdog via Modbus communication?
Unfortunately, for VIP410 relay, it is not possible to send the status of the watchdog via Modbus communication. There is no available Modbus address for the watchdog function.

施耐德電機Taiwan

Is it possible to send the status of VIP410 watchdog via Modbus communication?
Unfortunately, for VIP410 relay, it is not possible to send the status of the watchdog via Modbus communication. There is no available Modbus address for the watchdog function.