{}
搜尋常見問題
What are some of the benefits to an active front end in comparison to a classic approach front end with the Altivar 680/980 Series Variable Frequency Drives?
Issue:
Altivar 680/980 Series drives active front end benefits in comparison to a classic approach front end:
  • 12 pulse input
  • 18 pulse input
  • 6 pulse input with Harmonic filter

Environment:
All

Cause:
Harmonics

Resolution:
An active front end with the Altivar 680/980 Series Variable Frequency Drives provides a reduced foot-print size, higher efficiency standards and reduced EMI.

施耐德電機Taiwan