{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
Sepam 80 - saving MET148-2 temperatures to a log file when a protection trips occurs.
As of SFT2841 software version V15.0 and Sepam 80 firmware version V9.01, the temperatures measured by the MET148-2 module are not saved in the Tripping Context of the relay by default.

Please see the attached file for a workaround to this problem.

AEDL3

施耐德電機Taiwan

附件
Sepam 80_Saving_MET148-2_Temperatures_From_Trip_Event_v0.docx [291.36 KB]