{}
搜尋常見問題
Sepam 80 - pulse mode for Logic Outputs. What is the default pulse width for this mode?
For the Sepam 80 (and Sepam 60) relays, the pulse width for certain Logic Outputs can be set in SFT2841.

By default, the pulse width for the O1 tripping output is 200 milliseconds.  For certain other outputs on the MES120 input / output modules such as O101, this default width is 300ms.

Please see the attached file for details.  The results in the attached file were tested using firmware version V8.xx and SFT2841 software version V15.1.

AEDL3

施耐德電機Taiwan

附件
Sepam80_Pulse_Mode_Logic_Outputs_BFO-Case-31146496.docx [191.71 KB]