搜尋常見問題
Sepam ECI850 - how to check if the downstream Sepam relays on the RS-485 network have been disconnected?
For the Sepam ECI850 server, you can read the PhyHealth status value in the LPHD class.
If the Sepam devices defined in the ECI850 CID file have been disconnected from the RS-485 port and the number of retries has been exhausted, then this PhyHealth status will indicate a partial fault.
It is possible to add this data to a Dataset so that a Report could be generated from the ECI850 should the downstream Sepam devices become disconnected.
AEDL3
If the Sepam devices defined in the ECI850 CID file have been disconnected from the RS-485 port and the number of retries has been exhausted, then this PhyHealth status will indicate a partial fault.
It is possible to add this data to a Dataset so that a Report could be generated from the ECI850 should the downstream Sepam devices become disconnected.
AEDL3