搜尋常見問題
What can't I load an application to an XBTGK2330 via an SD card?
If you get this error while updating the application with an SD card on a Magelis XBTGK2330:
“Upgrading BSP – the auto-installer has detected an error; your application might not function correctly. Make sure target type is correct”.
For the XBTGK2330 with DOM after 1523 you must use Vijeo Designer V6.2 SP3.1 or higher on the initial download
“Upgrading BSP – the auto-installer has detected an error; your application might not function correctly. Make sure target type is correct”.
For the XBTGK2330 with DOM after 1523 you must use Vijeo Designer V6.2 SP3.1 or higher on the initial download
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: