Issue:
Can the ATV600 and ATV900 files be transferred from SoMove to the drive using the keypad?
Product Line:
ATV600 - ATV630, ATV640, ATV660, ATV680
ATV900 - ATV930, ATV940, ATV960, ATV980
Altivar Process
Environment:
All part numbers
Cause:
Not able to directly connect SoMove to the drive.
Resolution:
This process requires a USB to mini USB cable (not provided by Schneider Electric.
- Locate the mini USB port on the bottom right side of the VW3A1111 keypad and connect plug in the cable.
- Connect the cable to an available USB port on the PC. The PC should recognize the keypad as an external storage device.
- Open the file in SoMove.
- Go to the File menu and select Import/Export and then choose Export file.
The file name will have to match the Keypad's format so give it a File name of DriveConfPac#.cfg where the # is replaced by a number.
Save the file to the keypad's assigned hard drive under the DRVCONF folder. - Once you receive notice on your PC that "The Graphic Display Terminal file is exported successfully." you can disconnect the keypad from the cable and connect it to the drive.
- Navigate to Menu 7 [File Management] and then to Menu 7.1 [Transfer config file].
- Select Copy to the drive and then select the file name you exported from SoMove.
- Press OK to confirm and your file should transfer from the keypad to the drive memory.
- Power off the drive, and let the display go completely blank.
- Turn the power back on and verify the programming has changed.
發佈於: 施耐德電機Taiwan