Issue:
EPF1 fault on the Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
Probable Cause
EPF1 fault on the Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
Probable Cause
- Event triggered by an external device, depending on user.
- An external error has been triggered via Embedded Ethernet
- Check External Fault settings
- [Complete settings] -> [Error/Warning handling] -> [External error]
- External error assignment. If the assigned bit state is:
- 0: there is no external error.
- 1: there is an external error (EPF1)
- Check Embedded Ethernet settings
- [Communication] -> [Comm parameters] -> [Embd Eth Config]
- A faulty or duplicate address can cause conflicting issues.
- Try setting a different fixed IP address
- Check Network or PLC settings for any other conflicts
- Check for any possible electrical interferences
發佈於:施耐德電機Taiwan