搜尋常見問題
The Unity Help description for System Words %SW82 and %SW83 is incorrect for Unity Momentum PLC's
Goals and Symptoms
This Resolution explains the correct description of System Words 82 and 83 for a Unity Momentum PLC.
Facts and Changes
This Resolution explains the correct description of System Words 82 and 83 for a Unity Momentum PLC.
Facts and Changes
The description for System Words %SW82 and %SW83 are incorrect in Unity Help for Unity Pro versions 11.1 and lower.
It is corrected in Unity Help in Unity Pro versions 12 and higher.
It is corrected in Unity Help in Unity Pro versions 12 and higher.
Causes and Fixes
The correct description in Unity Help for Unity Pro versions 12 and higher is for Bridged messages.
Additional Information
>
>
發佈於:施耐德電機Taiwan
探索更多
系列:
產品:
探索更多
系列:
產品: