搜尋常見問題
What meter is used in the Powerpact 4 incoming metering extension enclosures MG64M, MG66M or MG88M?
The Powerpact 4 incoming metering extension enclosures MG64M, MG66M & MG88M come complete with a PM5110 meter.
The PM5110 has the following functionality:
The PM5110 has the following functionality:
- I, V, F Energy, PF
- THD and Min/Max readings
- Pulsed and Modbus outputs for energy monitoring
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: