我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
        
我们今天能为您提供什么帮助?
SEPAM with ACE850. Why I cannot access to the ACE850 Web Pages ?
 SEPAM with ACE850. Why I cannot access to the ACE850 Web Pages ?

Answer : The problem is on to the Application Versions installed in the laptop that are not compatible to access to the ACE850 Web pages .
The compatible Version installed on the laptop have to be :
For Internet Explorer Version < or = V11.0.38.
For Java only the V6.0.260 is availble to run with ACE850

IEDL3