搜尋常見問題
How do you set up the reference template on the ATV320 drive for pedestal mode?
Issue:
Setting up the reference template on the ATV320 drive for pedestal mode.
Product Line:
ATV32 and ATV320
Environment:
All
Cause:
Customer wants to have his 4-20mA reference signal follow 0 to 60hz even with a low speed setting on the drive of 10hz.
Resolution:
To adjust your speed reference for a 0-100% reference for 0-60hz please adjust the following.
Menu CONF - FULL - I/O -
Set BSP = bLS = Pedestal mode.
This will allow 0 speed to be 0 reference instead of using LSP as 0 reference.
Setting up the reference template on the ATV320 drive for pedestal mode.
Product Line:
ATV32 and ATV320
Environment:
All
Cause:
Customer wants to have his 4-20mA reference signal follow 0 to 60hz even with a low speed setting on the drive of 10hz.
Resolution:
To adjust your speed reference for a 0-100% reference for 0-60hz please adjust the following.
Menu CONF - FULL - I/O -
Set BSP = bLS = Pedestal mode.
This will allow 0 speed to be 0 reference instead of using LSP as 0 reference.
發佈於:施耐德電機Taiwan
附件
探索更多
系列:
探索更多
系列: