{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What fan mode settings are available on the ATV630/660?
Issue:
Customer needs adjust fan strategy on the ATV630/660?

Product Line:
ATV630, ATV660

Environment:
All

Cause:
Would like to know what fan options are available

Resolution:
The fan modes are located in [Complete settings] -> [Maintenance] -> [Fan management].
Modes available are Standard (factory setting), Always, Economy, and Never.
When in Standard mode, the fan runs while the motor is running and may continue to run after motor stops depending on the drive's thermal needs.
In Economy mode, the fan runs only to satisfy the minimum thermal needs of the drive.
If [Fan Mode] FFM is set to [Never] Stp, the fan of the drive is disabled. (*This is not recommended. Service life of the internal electrical components is reduced.)

Fan Mode FFN

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: