搜尋常見問題
Is it possible to use SH motors with LXM32 ?
Yes, it is possible, but only with LXM32M and with analog encoder card added to LXM32M. Data in encoder of SH motor are not compatible with LXM32, so the only option is to configure LXM32M as for 3rd party motor.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: