搜尋常見問題
Can we guarantee Type 1 or Type 2 coordination for motor control and protection using EasyPact CVS circuit breaker?
Using the EasyPact CVS circuit breakers equipped with magnetic MA protection we can assure Type 1 coordination in combination with the contactors and relays from the attached table.
The product combinations from the attached table must be followed to assure Type 1 coordination.
The product combinations from the attached table must be followed to assure Type 1 coordination.
發佈於:施耐德電機Taiwan
附件
探索更多
系列:
探索更多
系列: