{}
搜尋常見問題
Can the side slam latches of a NetShelter SX cabinet be locked or disabled so they can only be opened from inside the cabinet?
Issue:
The NetShelter SX has side slam latches that unlock from outside the cabinet.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
A concern for security would most likely create the need to 'freeze' the side locks.

Resolution:

See attachment below.

施耐德電機Taiwan

附件
20180227 How to Permanently Lock the NetShelter SX Side Panel.pdf [37.94 KB]
探索更多
系列:
可能有幫助的文章
探索更多
系列: