What is the IP degree of protection XALD/K enclosures following the Harmony "+" launching ?The global range is IP66, IP67, IP69 and IP69K, find a declaration of conformity in attachment.
發佈於:施耐德電機Taiwan
附件18-006 C&S Harmony d22mm heads IP66, IP67, IP69, IP69K.pdf [44.72 KB]