{}

我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
Freq. inverter ATV Process on Profinet network. How read/write more than 8 PZDs? The SoMove Eth/IP scanner displays the max of 8
YEs, it is possible to map up to 16 input and 16 output PZDs on profinet, profile 107. Somove does not show profinet mapping variables. Variables have to be mapped in PLC profinet configuration.
Eth/IP scanner shows mapping for eth/ip communication, but if you use profinet, then whatever variables are seen in ethernet IP scanner they are irrelevant. Somove shows a kind of default scanner prepared for eth IP.
Tested in TIA portal v 15, S7-1500, ATV930.