{}
搜尋常見問題
How do you perform a Factory reset on the ATV12 drives?
Issue:
ATV12 back to factory configuration

Product line:
Altivar 12, ATV12

Environment:
all

Cause:
n/a

Resolution:
Navigate to the ConF menu using the dial. Push the Enter button (the dial is the Enter button). Scroll down to FCS and push Enter.
The display should say nO. Change the dial to InI. Push and hold the Enter button for 2-3s. The display will change back to nO when completed.

Note: A factory reset cannot be completed when the drive is running. The drive must be stopped.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: