{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What color are the NetShelter SX pallet brackets?
Issue:
The customer is hoping to use the pallet brackets to mount the cabinet to the floor.

Product Line:
NetShelter SX cabinets

Environment:
All models, all serial numbers.

Cause:
The customer wants to know if the pallet bracket color matches the cabinet color.

Resolution:
The color of the pallet brackets used in the NetShelter SX match the color of the cabinet.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: