搜尋常見問題
Dimensions of GV2APN01 / GV2APN02 shaft handle used for GV2P and GV2ME Motor starters?
The metallic shaft included in ref. GV2APN01 / GV2APN02 has dimensions 6 x 6 x 315mm - see page 1/6 of Attachment1.
The shaft is cuttable. Minimal and maximal distance between enclosure door and back of GV2 circuit breaker is shown on page 2/6 of Attachment1.
The shaft is cuttable. Minimal and maximal distance between enclosure door and back of GV2 circuit breaker is shown on page 2/6 of Attachment1.
發佈於:施耐德電機Taiwan
附件
探索更多
系列:
探索更多
系列: