搜尋常見問題
What can cause an InF0 or internal error 0 fault on the ATV630 and ATV930 Process drives?
Issue:
InF0 or internal error 0 fault on the ATV630 and ATV930 Process drives.
Product Line:
ATV630 and ATV930 Process drives
Environment:
All
Cause:
Internal control block CPU error.
Resolution:
Internal CPU error
Principle:
Internal control block CPU error.
Remedies:
- restart the drive (switch the drive OFF / ON)
- change the control block.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)