{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What is the dc component for the HV circuit breakers ?
The DC component for the ranges of circuit breakers HVX Evolis, EasyPact EXE, LF, and SF is 30%.
This value is in accordance with the IEC 62271-100.
The time constant is 45 ms.

Due to special applications such as generator applications, the requirement of DC% will be much higher.
For HVX  generator version the DC% can be up to around 75% with a time constant 133 ms for 100% short circuit current switching.
The test was performed according to IEEE C37.013 or IEC_IEEE 62271-37-013.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: