搜尋常見問題
INTERNAL: MGE EPS 6/7/8 AMUZ Display Normal status message appears incorrect
Issue:
MGE EPS 6/7/8 AMUZ Display Normal status message appears incorrect
Product line:
EPS 6000 / 7000 / 8000
Environment:
All models, all serial numbers with GUI
Cause:
Normally in NAM the GUI will indicate Normal Load Protected UPS online
This can be changed by changing the language the display uses to provide information.
If UK English is chosen the verbiage changes to Normal Load Protected Power Supply Okay, it means the same thing just says it in a slightly different way.
Resolution:
In the menu change language to NAM (North American) English and that should bring it back to the expected verbiage.
Follow instructions in Operations/User Manual
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: