搜尋常見問題
How to discover and add the devices in Ecoreach that are connected as Modbus slaves to the gateway?
To discover the device click on the "Launch Device Discovery" on the Ecoreach home screen to discover the Gateway. Once the gateway is discovered enter the Modbus slave address in the "Address" section and then select the required devices by clicking on the checkbox next to the IP address of the discovered device and click on "Add Devices" to add the devices to the Ecoreach project.
Please refer to the attached document for details.
Please refer to the attached document for details.
發佈於:施耐德電機Taiwan
附件
探索更多
系列:
探索更多
系列: