Issue:
Error "1031 cannot store the configuration to the device" on SoMove.
Product Line:
Altivar ATV320
Environment:
All serial numbers
Cause:
The error popped up in SoMove when customer tried to download drive program to his PC.
Resolution:
Checked to see customer uses function blocks. The function blocks can be turned off using SoMove. In SoMove, go to Parameters in menu bar, click on FULL and select Function Blocks, then under FBCD (FB command) change to "Stop". Restarted SoMove after the change.
發佈於: 施耐德電機Taiwan