STW6 is a Web HMI that accesses Web servers on an intranet and displays screens. It has the following characteristics.
The following features have not been supported yet.
Restriction
HMISTW6 is not compatible with the features below.
- Compatible with an HTML5 server supporting Java Script.
- Proxy cannot be used.
- Configure a system of multiple Web HMI units with a daisy chain.
The following features have not been supported yet.
- Access to Web servers on Internet
- Access to HTML5 pages on an external storage
Restriction
HMISTW6 is not compatible with the features below.
發佈於:施耐德電機Taiwan