{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
How to make a momentary switch with a delay in Vijeo Designer?
Issue:
The momentary switch resets too quickly for the PLC to detect the state change from ON to OFF.

Product Line:
Vijeo Designer (all versions)

Resolution:
When the native Momentary On switch does not set a bit long enough for your application (possibly due to slower communications), it is possible to create your own Momentary On switch with a desired delay to wait before resetting the bit. Here we will provide a procedure on how to build this in Vijeo Designer.

1) On the Panel, draw a switch.
2) Set the Operation to "Bit"
3) First select the "Set" Operation
4) Assign your desired variable to the "Destination" Field. For this example, we will create BOOL01.
5) Press the "Add" button.
6) Next, set the Operation to "Delay".
7) In the Field "Delay Time", enter a static value or a mathematical expression. For this example, we will enter 2 (seconds).
8) Press the "Add" button.
9) Next, set the Operation to "Bit"
10) Select the "Reset" Operation
11) Assign BOOL01 to the "Destination" Field.

With the above procedure, you will create a Momentary On switch that sets a bit "BOOL01" for 2 seconds and then resets it afterwards


施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: