搜尋常見問題
Why a new hardware has been design on M580 PLC range with FW V2.90?
A new Hardware has been design to replace the front panel Ethernet switch embedded inside this PLC range.
In the past we have obeseved a lake of robustness on this switch. Although the occurance of the problems was low, it was considered necessary to improve the robustness of this switch.
In 2019 M580 Safety CPUs don't support this new hardware so M580 Safety CPUs don't support SV2.90 in 2019.
In the past we have obeseved a lake of robustness on this switch. Although the occurance of the problems was low, it was considered necessary to improve the robustness of this switch.
In 2019 M580 Safety CPUs don't support this new hardware so M580 Safety CPUs don't support SV2.90 in 2019.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: