搜尋常見問題
How to obtain scan execution times in M340 and Quantum PLC
Issue
What are scan execution times in M340 and Quantum PLC
NOTE (definitions):
- The amount of time it takes to perform one cycle is referred to as scan time
- Cycle means perform all configured, programmed and enabled activities in a fixed sequence as fast as possible
Product Line
Unity Pro (software)
M340, Quantum (PLC)
Environment
System Addressing
Cause
Trouble shooting purpose
Resolution
Scan execution times can be obtained using system objects:
What are scan execution times in M340 and Quantum PLC
NOTE (definitions):
- The amount of time it takes to perform one cycle is referred to as scan time
- Cycle means perform all configured, programmed and enabled activities in a fixed sequence as fast as possible
Product Line
Unity Pro (software)
M340, Quantum (PLC)
Environment
System Addressing
Cause
Trouble shooting purpose
Resolution
Scan execution times can be obtained using system objects:
- %SW30 last scan
- %SW31 longest scan
- %SW32 shortest scan
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: