搜尋常見問題
Is my Speed D Switchboard rated 80% or 100%
The Class 2710 Speed D Switchboard is rated for 80% of it maxi um rating or Over Current Protective Device (OCPD). Currently there is not an option for a 100% rated Speed D Switchboard.
For a 100% rated Switchboard application a Power-StyleTM QED-2 Series Switchboard will need to be considered.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: