{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站

搜尋常見問題

How to convert DINT&DWORD type to Bit type in Unity Pro and ECE?

  1. Issue
Customer wants to convert DINT variable and DWORD variable to Bit, but there is no such EFB in the library, only WORD_TO_BIT and BYTE_TO_BIT found
  1. Product Line
Unity Pro, Control Expert
  1. Environment
Unity Pro, Control Expert
  1. Resolution
Here is one of the example DFB to convert the  “dint_to_bit” and “dword_to_bit” which can be used to convert the variable type.
I can share you the source code for your reference.


施耐德電機Taiwan

附件

dint_dword_to_bit.rardint_dword_to_bit.rar [2.78 KB]
探索更多
系列:
EcoStruxure Control Expert (Unity Pro)
探索更多
系列:
EcoStruxure Control Expert (Unity Pro)