{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站

搜尋常見問題

What are S1, S2,and S3 in the LH4N2 wiring diagram?

Issue:
S1, S2 and S3 buttons wiring diagram indication in LH4N2.

Product Line:
LH4N

Environment:
All

Cause:
Control wiring circuit

Resolution:
The S1, S2, and S3 are switch designations in the recommended wiring schemes. When these switches are wired as indicated the S1 is for freewheel stop operation, S2 is for soft start operation FWD, and S3 is for soft start REV.




photo 22

施耐德電機Taiwan

附件

LH4N Soft Starter Installation Manual.pdfLH4N Soft Starter Installation Manual.pdf [143.1 KB]
探索更多
系列:
探索更多
系列: