搜尋常見問題
Which fonts are compatible with our Web Terminal HMISTW6xxx?
In some cases, when the Web terminal is connected to a server web, the web page displayed is different than the original one. This article will describe compatible fonts in HMISTW6
This article is applicable for Web Terminal HMISTW6xxx, with the firmware FWV1.1.0,
Currently, in the firmware version FWV1.1.0, there are 4 font familly installed
![Annotation 2021-02-18 105755.jpg](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009INosQAG&oid=00DA0000000abSmMAI)
The following table describes the font support status in different software version.
![Annotation 2021-02-18 110134.jpg](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009INotQAG&oid=00DA0000000abSmMAI)
This article is applicable for Web Terminal HMISTW6xxx, with the firmware FWV1.1.0,
Currently, in the firmware version FWV1.1.0, there are 4 font familly installed
The following table describes the font support status in different software version.
發佈於:施耐德電機Taiwan
探索更多
產品:
探索更多
產品: