搜尋常見問題
Which are the IP address set by default on HMI Harmony HMISTM6BOX (Gateway Box Model)?
The HMISTM6BOX is a gateway which can be used with or without screen touch. By default the HMISTM6BOX is delivered without touch screen.
The goal of this FAQ is to provide you the default IP address configured by default in our product.
The FAQ is applicable for HMISTM6BOX and EcoStruxure Operator Terminal Expert 3.2 (minimum)
![test test](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000007uePGQAY&oid=00DA0000000abSmMAI)
The goal of this FAQ is to provide you the default IP address configured by default in our product.
The FAQ is applicable for HMISTM6BOX and EcoStruxure Operator Terminal Expert 3.2 (minimum)
發佈於:施耐德電機Taiwan
探索更多
產品:
探索更多
產品: