Why are HMISTU655 and HMISTU855 no more visible in the list of Target Models into Vijeo Designer 6.2 SP11?
This FAQ concerns HMISTU655, HMISTU855, HMIS5T.
HMISTUx55s manufactured before 2012/03/12 (i.e. not marked with the label reference HMIS5T on the rear module) are no longer supported in VJD 6.2 SP11 and require a previous version of Vijeo Designer for their maintenance.
Summary:
-Labels with HMISTUx55 on rear module require Vijeo Designer 6.2 SP10 or less
-Labels with HMIS5T on rear module can be used also with Vijeo Designer 6.2SP11 or more
發佈於:施耐德電機Taiwan