搜尋常見問題
EcoStruxure Automation Expert [21.1]:How to resolve the issue "Deploy Plugin AvevaServerPlugin not installed" ?
This knowledge base helps the user to resolve the "Deploy Plugin AvevaServerPlugin not installed" issue that comes under the Deploy and diagnostic tab when the AVEVA_SERVER device is being used in the project?
The error message shows as below highlighted in Yellow color
The issue is happening as the mandatory plugin required for AVEVA_SERVER device is not installed in the machine.
The AvevaServerPlugin can be installed either by reinstall/repair the Ecostruxure Automation Expert
The user needs to select the "AutoBuild AVEVA InTouch OMI" for any of the highlighted selections and complete the installation procedure.
NOTE: The Default selection is "This Feature will not be available".Hence plugin is not getting installed by default.