Does TeSys Giga Contactor can be used in functional safety application (for SIL1 and SIL2)?
TeSys Giga Contactors can be use in a SIL1 Safety loop in 2 or 5 wires mode with the safety stop control wire on X3 port. SIL2 Level can be reached with redundancy.