{}

我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What are IDLF faults on a ATV680 drive?

Issue:

IDLF faults on a ATV680 enclosed product

 

Product Line:

ATV680

 

Environment:

IDLF faults

 

Cause:

n/a

 

Resolution:

 

When the device is in IDLE mode and you send a run command, but the device does not start to charge the bus within the adjusted energy saving timeout [idLt] (Factory settings: 5s // 8s for ATVx80 and ATVxB0), then the device will trip with IDLF.

Probable cause: The mains voltage is missing and the device cannot charge the DC Bus.

Remedies :Check mains voltage and ensure its availability. Check the DC bus voltage