搜尋常見問題
Can you tell me the size of a 40hp soft-start in an model 6 bucket [
Issue:
Wants the space required to fit a 40HP ATS22 bucket in Model 6 MCC
Product Line:
Model 6 MCC
Environment:
ATS22 bucket
Cause:
Space requirement
Resolution: The 40HP 480V ATS22 requires 18", but options may increase base size.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: