搜尋常見問題
How to configure EIP buscycle with BMED581020 (IEC 61499)
Context: Example BusCycle EIP configuration (IEC 61499) between BMED581020 and BMEP586040.
![EIP configuration BMED581020 EIP configuration BMED581020](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CW5QaQAL&oid=00DA0000000abSmMAI)
![BMED581020 EIP configuration buscycle BMED581020 EIP configuration buscycle](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CW5QbQAL&oid=00DA0000000abSmMAI)
BusCycleTime must be greater than RPI O -> T + RPI T -> O
Example:
BusCycleTime (80ms) >> RPI O -> T (30ms) + RPI T -> O (30ms)
Note: if there are several devices, take the highest RPI O -> T and RPI T -> O.
Product line:
EAE, EIP, Buscycle, Time, BMED581020, IEC 61499
Environment:
Windows, EcoStruxure Automation Expert 22.0
BusCycleTime must be greater than RPI O -> T + RPI T -> O
Example:
BusCycleTime (80ms) >> RPI O -> T (30ms) + RPI T -> O (30ms)
Note: if there are several devices, take the highest RPI O -> T and RPI T -> O.
Product line:
EAE, EIP, Buscycle, Time, BMED581020, IEC 61499
Environment:
Windows, EcoStruxure Automation Expert 22.0
發佈於:施耐德電機Taiwan
探索更多
產品:
探索更多
產品: