搜尋常見問題
What are the part number of the terminal blocks needed for the modules of the Modicon MC80 controllers?
Issue:
Do not know which is the part number of the terminal blocks needed for my MC80 controller.
Product Line:
BMKC8020310, BMKC8020301, BMKC8030311, MC80 PLC
Resolution:
For each of the available MC80 controllers, the required terminal blocks, and the amount of each them, is as follows:
► BMXC8020301
1x - BMXFTB20xx
1x - BMXFTB28xx
► BMKC8020310
1x - BMXFTB20xx
1x - BMXFTB28xx
► BMKC8030311
1x - BMXFTB20xx
2x - BMXFTB28xx
Do not know which is the part number of the terminal blocks needed for my MC80 controller.
Product Line:
BMKC8020310, BMKC8020301, BMKC8030311, MC80 PLC
Resolution:
For each of the available MC80 controllers, the required terminal blocks, and the amount of each them, is as follows:
► BMXC8020301
1x - BMXFTB20xx
1x - BMXFTB28xx
► BMKC8020310
1x - BMXFTB20xx
1x - BMXFTB28xx
► BMKC8030311
1x - BMXFTB20xx
2x - BMXFTB28xx
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: