{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What is the difference between NFC and RFID for Evlink Pro AC ?
RFID (Radio frequency identification) systems consist of a reader with an antenna and a transponder. There are three different RFID frequency ranges : low frequencies, high frequencies and upper high frequencies. RFID can be used for long distances (for example in highway tolls)

NFC is based on RFID protocols. It operates on the same high frequency as RFID. Because of the short read range limitations, NFC devices have to be in very close proximity and are used for short distances (for example in phones).

Therefore, the main difference between NFC and RFID is the distance at which they can be used.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: