Issue
I am trying to determine voltage drop from a 2-10VDC signal generated by a BMXAMO0410 AO Module.
What is the current generated at the device to provide the 10VDC signal?
Product Line
X80 Analog I/O Modules - BMXAMO0410
Environment
Electrical characteristics
Resolution
For the BMXAMO0410, per channel, the minimum load impedance for voltage output is 1 kOhm.
Where the min load impedance is 1 kOhm, that means at +10VDC, the max current draw cannot exceed 10mA. 10vdc/1000 ohm= 10mA.
Also see: https://en.wikipedia.org/wiki/Output_impedance
發佈於:施耐德電機Taiwan