Recommandations: if the scale is located in an environnement with vibrations there is a logical filter which can be adjust in the DTM of the PMESWT0100.
- In most of the cases, we adjust the low-pass cut off frequency on 15hz or 20 hz.
- The AD converter rate which means number of sampling per second can be adjusted to a value "200".
- At least we recommand to adjust the Mean-filter setting to 16. This performs a moving average of the weight.
發佈於:施耐德電機Taiwan