Issue:
How do I start-up/turn on BE900G3 and BE1050G3?
Product Line:
BE900GE and BE1050GE
Environment:
All Serial Numbers
Steps / Procedures:
1. Connect the internal battery (The Back UPS is shipped with one battery cable disconnected).
Follow the series of steps stated below:
2. And when the battery is connected successfully, plug it into the Utility or AC main source.
3. Press the POWER button. It will illuminate green, and a single short beep indicates that the Backups is on and helping to provide protection for connected equipment.
Additional inputs:
* Self-Test only occur upon start up.
* Intentional manual self-test is not applicable for this particular product.
* Battery replacement for Backups BE900G3 is RBC17 and BE1050G3 is APCRBC164.
發佈於:施耐德電機Taiwan