搜尋常見問題
video: How to setup S2 Redundancy communication between Altivar and Siemens redundant PLCs ? (using PROFINET module VW3A3647)
This video explains how to setup S2 Redundancy communication between Altivar and Siemens redundant PLCs using the PROFINET module VW3A3647 in TIA Portal.
🔔 Timestamps :
00:15 - Programming
04:02 - Compile of the project
04:34 - Transfer the project
➡️ For more information see :
• GSDML FILES : PROFINET_GSDML_VW3A3647
• ATV900 PROFINET Manual - VW3A3647 - BQT46620
• ATV600 PROFINET Manual - VW3A3627 - EAV64331
🔔 Timestamps :
00:15 - Programming
04:02 - Compile of the project
04:34 - Transfer the project
➡️ For more information see :
• GSDML FILES : PROFINET_GSDML_VW3A3647
• ATV900 PROFINET Manual - VW3A3647 - BQT46620
• ATV600 PROFINET Manual - VW3A3627 - EAV64331
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: